Technical FAQs

Ask a Question

What is the Selection Criteria of EDS for TeSys T LTMR Controller Variants?

There are four EDS files corresponding to the four possible configurations of the TeSys T Motor
Management Controller system:

SE TeSys T MMC L EIP 
A TeSys T Motor Management Controller system without an expansion module, configurable via the HMI port. This variant enables you to preserve your local configuration.
SE TeSys T MMC L EV40 EIP 
A TeSys T Motor Management Controller system with expansion module, configurable via the HMI port. This variant enables you to preserve your local configuration.
SE TeSys T MMC R EIP
A TeSys T Motor Management Controller system without expansion module configurable via the network.
SE TeSys T MMC R EV40 EIP 
A TeSys T Motor Management Controller system with expansion module configurable via the network.
 
Was this helpful?
What can we do to improve the information ?