Technical FAQs

Ask a Question

What is the Basic difference between BMXNRP0200 & BMXNRP0201?

These are the some difference

BMXNRP0201:-
Fiber Converter SM/LC 2CH 100Mb
* Optic fiber type: Single Mode
* Operating Distance: 0...15000 m
* Attenuation: -15...-8 dB (9/125 µm)
* Rise/fall time: 2.5 ns
* Receiver sensitivity: - 31...- 8 dBm
  
BMXNRP0200:-
 Fiber Converter MM/LC 2CH 100Mb
* Optic fiber type: Multi Mode
* Operating Distance: 0...2000 m
* Attenuation: -23.5...-14 dB (50/125 µm)
           -20...-14 dB (62.5/125 µm)
* Rise/fall time: 3 ns
* Receiver sensitivity: - 31...- 14 dBm
 
Was this helpful?
What can we do to improve the information ?