Browse FAQs

What is the part number of the locking or ring nut for Vario and Mini Vario Handle Operators?

Published date: 06 August 2019

Issue:
Vario and Mini Vario single hole lock/ring nut

Product Line:
UL 508 Motor Disconnect Switches

Environment:
Single hole mount Mini-Vario and Vario™ Assembled and Enclosed Switches

Resolution:
Part number is KZ30 for the ring nut only.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.