Browse FAQs

Does the HMISTU series have a built-in terminating resistor?

Published date: 14 May 2019

Issue:
Does the HMISTU have a built-in terminating resistor on the RS485 COM port?

Product Line:
Magelis HMISTU, HMIS5T

Resolution:
No, the HMISTU series does not have a built-in terminating resistor on the RS485 COM port. If a terminating resistor is required, it should be built into the communication cable that is used between the HMISTU and the serial device.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.