Search FAQs
How to connect to a SmartX server (AS-P/AS) using the IP network in EcoStruxure Building Operation.
Please refer the below procedure:
1. In Device Administrator, click Servers and then click Add server.
2. In the Connect to a server dialog box, in the Server address box, type the IP address or the host name of the SmartX server.
3. Enter the password in one of the following ways:
1. In Device Administrator, click Servers and then click Add server.
2. In the Connect to a server dialog box, in the Server address box, type the IP address or the host name of the SmartX server.
3. Enter the password in one of the following ways:
- Type the password for this SmartX server.
- Select Use site specific device password to log on using the password specified in the Device log on options dialog box.
Released for:Schneider Electric India
Explore more
Explore more