Technical FAQs

Ask a Question

What are the pins to apply rated 24V power supply to disable 'dIS' state of the drive.

Dis state on drive means ‘Switched On Disabled’ and it is not an error.
If not using power safety function, then apply 24V DC to PWRR_A and PWRR_B at pins 37 & 38 of CN1 to disable the state.



 
Was this helpful?
What can we do to improve the information ?