Browse FAQs

What is the default IP Address Assignment of BMENOS0300 module

Published date: 01 June 2019

If the DHCP server in the CPU is not configured to supply the BMENOS0300 module with an IP address, the module will assign itself an IP address based on its MAC address, as follows:
10.10.x.x
Where x.x represents the decimal version of the last two (fifth and sixth) octets of the MAC Address.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.