Technical FAQs

Ask a Question

What is the replacement for Part Number ILS1F852S2142?

Issue
What is the replacement for Part Number ILS1F852S2142?

Product Line
Lexium Integrated Drives

Resolution
The Part Number ILS1F852S2142 (Lexium Integrated Drive) is a special proprietary model specifically made for specific OEM machine builders.
It is not available for purchase directly from Schneider Electric.
 
Please contact the OEM system builder of the machine/device that this motor is incorporated into in order to obtain a spare or replacement.
Was this helpful?
What can we do to improve the information ?