Technical FAQs

Ask a Question

What are the LED status of ATV61/71.

Please find the below status of LED.
LED 2.1 (blinking) - Receiving data
LED 2.2 (Off) - Not transmitting data 
LED 2.3 (Solid red) - Ethernet fault present 
LED 2.4 and 2.5 (solid Green) - IP address configured, 100MBPS baud rate 
 
Was this helpful?
What can we do to improve the information ?