Technical FAQs

Ask a Question

How to flash the M251 firmware

Issue:
How to flash the M251 firmware

Product Line:
M251

Resolution:
- Start by launching 'Controller Assistant'
- Select 'Update firmware'
- Choose the M241/M251 and select the latest firmware
- Enter the IP, Subnet and Gateway you would like the M251 to have once the flashing is done
- Click on 'Write to controller'
- Find the controller in the list and double click on it, then hit 'Connect'
Was this helpful?
What can we do to improve the information ?