Technical FAQs

Ask a Question

How to upload a program from an M251 controller

Issue:
How to upload a program from an M251 controller

Product Line:
M251

Resolution:
- Start by launching SoMachine
- Select 'Connect Controller'
- If controller is powered and connected by USB, it shows up in the list.
- Select it and click 'Upload project from controller'
- Select where to save the uploaded file on your PC and select 'Yes' to open it.
- You can now access the project code
Was this helpful?
What can we do to improve the information ?