Technical FAQs

Ask a Question

Is the AR9000RAMP reusable? If so, how many times can it be reused?

Issue:
There is no documentation stating how many times the ramp can be reused. 

Product Line:
NetShelter SX HS

Environment:
All versions and serial ranges.

Cause:
It is unknown whether the AR9000RAMP is reusable. 

Resolution:

Yes, the AR9000RAMP is reusable. 
Although there is no set number of times it may be reused, the Installation Manual has the following statement: 

 
Was this helpful?
What can we do to improve the information ?