Technical FAQs

Ask a Question

How to properly calibrate the touchscreen on a HMIBMU series

Issue:
How to properly calibrate the touchscreen on a HMIBMU series

Product Line:
Magelis iPC, HMIBMU, HMIBMI

Resolution:
When calibrating the touchscreen of an HMIBMU or HMIBMI series, ensure not to use the Windows calibration tool. Instead, look for the PenMount Control Panel and use the calibration tool of that application. It provides the option for 25 points of calibration. By using 25 points, it gives the touchscreen a more accurate calibration.
 
Was this helpful?
What can we do to improve the information ?