Technical FAQs

Ask a Question

To mount equipment at varying depths in a NetShelter SX cabinet should additional original full height rails be used, or should a recessed rail kit be used?

Issue:
Equipment with different mounting depths needs to be mounted into a cabinet. 

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Need to know if the recessed rail kits must be used between the original full height rails, or if full height replacement rails will work. 

Resolution:

Always use recessed rail kits to install equipment of differing depths. 
The original full height mounting rails should be used for the front and rear rails.
Any rails installed between the original full height rails should be the recessed rail kits. 

 
Was this helpful?
What can we do to improve the information ?