Technical FAQs

Ask a Question

How to check Online Status of the SmartX Server in EBO.

To check the online status of the SmartX server follow the below steps.
1. In WorkStation, in the System Tree pane, expand the Enterprise Server folder, for example, Server 1.
2. Expand the Servers folder.
3. Verify the SmartX server status:
    • The SmartX server icon displays if the SmartX server is online.
    • A red symbol displays in the SmartX server icon if the SmartX server is offline.
4. Also, View the alarm status.
 
Was this helpful?
What can we do to improve the information ?