Technical FAQs

Ask a Question

Why EcoStruxure BMS Server Failed to Create Backup Set in EBO.

Kindly follow the below steps:-

1. Ensure that a backup is not already in progress.
2. Ensure that the backup set size does not exceed the single SmartX server backup partition disk space. If the disk space is exceeded, the probable cause can be an exceeded amount of trend logs. 
3. Check for an error in one of the modules participating in the backup, or in the backup module itself.
 
Was this helpful?
What can we do to improve the information ?