Technical FAQs

Ask a Question

What need to do when Network Licenses are Broken in EBO.

To repair a network license follow the below steps:-

1. In License Administrator, click the Licenses view.
2. Select the network license that you want to repair.
3. On the Licenses toolbar, click the Repair license button.
4. In the Licenses dialog box, click Yes.
5. In License Administrator, click Close.
6. Click Restart now to restart the License Server and make the repaired licenses available for checkout.
 
Was this helpful?
What can we do to improve the information ?