Technical FAQs

Ask a Question

Why cannot Mass create Trend Logs or Alarms in EBO.

Ensure that the alarm or trend log is suitable for the selected objects or properties. If no alarm or trend log is suitable for your combination of objects or properties, the Create Object wizard does not open. In addition, also ensure that the selected objects or properties have the same unit or no defined unit. If you have selected objects or properties with different units, the Create Object wizard does not open
 
Was this helpful?
What can we do to improve the information ?