Technical FAQs

Ask a Question

Can I connect both computer and ATV630 or ATV930 drives to the HMI at the same time?

Issue:
Can I connect both computer and ATV630 and ATV930 drives to the HMI at the same time?

Product Line:
ATV630 ATV930

Environment:
All serial numbers

Cause:
N/A

Resolution:
It's not possible to connect computer and ATV630 or ATV930 at the same time to the HMI.  
Was this helpful?
What can we do to improve the information ?