Technical FAQs

Ask a Question

On the ATV630 and ATV930, which option should I select under HMI command in SoMove to switch between terminal or HMI on the keypad?

Issue:
On the ATV630 and ATV930, which option should I select under HMI command in SoMove to switch between terminal or HMI on the keypad? 

Product Line:
ATV630 ATV930

Environment:
All serial numbers

Cause:
Customer didn't want to change on the keypad.

Resolution:
In SoMove, select "Cmd/ref copied c/over" under HMI command.  
 
Was this helpful?
What can we do to improve the information ?