Technical FAQs

Ask a Question

Should we use fuses for the control power of meter.

You should include fuses at the control power terminals.
L1 and L2 are non-polarized. If using an AC power supply with  neutral, connect neutral to the meter’s L2 terminal.
Always use a fuse on L1. Fuse L2 when connecting an ungrounded neutral to the control power. If using a control power transformer,
fuse both primary and secondary sides of the transformer. The fuses / circuit breakers must be rated for the installation voltage and sized
for the available fault current.

Kindly find the attachment for the instruction.


 
Was this helpful?
What can we do to improve the information ?