Technical FAQs

Ask a Question

What does it mean if STS led of STBNIP2311 is blink 8 times

The STS LED binking 8x is related to a "TR_EVT_FATAL_ERROR" event, which could be caused by the modules inability to obtain a MAC address or to obtain configuration data. 
It means that the module is faulty and it has to be replaced.

 
Was this helpful?
What can we do to improve the information ?