Technical FAQs

Ask a Question

what is the isolation voltage between the housing and the electronics of the XT112S1PCL2 capacitive sensor

XT112S1PCL2 capacitive sensor in plastic casing supplied in Ue=24Vdc, according to the IEC 60947-5-2 standard, rated isolation voltage is 75Vdc
Was this helpful?
What can we do to improve the information ?