Technical FAQs

Ask a Question

Do all ATV12 Drives come with EMC Filter

It's depend of ATV12 range : 
  • ATV12.....F1 and ATV12......M3 drives are designed without embedded EMC filter.
  • ATV12.....M2 have built in EMC filter. And it's possible to deactivate it with the IT jumper on the product.
Was this helpful?
What can we do to improve the information ?