Technical FAQs

Ask a Question

What do we do when the HMISTO7 shows an error while booting?

Issue:
What do we do when the HMISTO7 shows an error while booting?

Product Line:
HMISTO7 Series

Resolution:
On the screen with the error, there is a button labelled "USB", if you press that button while a USB Memory stick containing a file system image is inserted, it will take you to the hardware configuration screen and allow you to load from the USB stick. This will help you install the program and stop this error from appearing.
Was this helpful?
What can we do to improve the information ?