Technical FAQs

Ask a Question

How to change device type in RemoteConnect with an existing project?

  1. Open Project using RemoteConnect.
  2. Write click on the SCADAPack x70 Controller Settings - DeviceDTM
  3. Select Additional Functions>Project Settings
  4. A project settings window will pop up and under Device Type select the correct controller type.

 
Was this helpful?
What can we do to improve the information ?