Technical FAQs

Ask a Question

How to edit or change configuration options in RemoteConnect with an existing project?

  1. Open project using RemoteConnect.
  2. In oflline mode, write click on  SCADAPack x70 Controller Settings - DeviceDTM
  3. Select Additional Functions>Project settings
  4. A window Project settings will pop up and then edit or change the required configuration options.


5. Then Write program back to the RTU to make changes on the configuration options parameters.
 
Was this helpful?
What can we do to improve the information ?