Technical FAQs

Ask a Question

How to access "ConF" Mode in ATV12 using master password via Somove software

ATV12 master password is 2663. 

It can be entered on the COP parameter or using somove software. 

Connect the drive to PC using somove. It will ask for password. Enter master password 2663 to access all the parameter settings.
Now the drive is also available for factory reset using somove. 
Was this helpful?
What can we do to improve the information ?