Technical FAQs

Ask a Question

Why M340 "upload option" disable in Unity Pro XL

If upload option is disable in Unity Pro XL, check the below path:

Tools ---> General ----> PLC Embedded Data

Check the "Upload Information". If it is selected, program transfer from the PLC to PC cannot be done. Also in Unity Pro XL "No Upload Info" is shown as per attachment. 
Was this helpful?
What can we do to improve the information ?