Technical FAQs

Ask a Question

For which application Micrologic 5 A-Z trip units are used.

Micrologic 5.2 A-Z and 5.3 A-Z are dedicated to 16 Hz 2/3 networks.They use  suitable sampling frequency. The protection settings are identical to those of Micrologic 5 A. They also offer a current-measurement function for this specific frequency.
 
Was this helpful?
What can we do to improve the information ?