Technical FAQs

Ask a Question

What is the purpose of using Micrologic 2 AB for Compact NSX.

Micrologic AB trip units are used in public distribution systems to limit the current supplied according to the consumer's contract. They are available in 100, 160, 240 and 400 A ratings and are supplied with a lead-seal device to protect the settings.
 
Was this helpful?
What can we do to improve the information ?