Technical FAQs

Ask a Question

Is access to micrologic of Compact NSX protected by password.

Remote access to data on Micrologic trip units is protected by password. Remote access includes:

 The communication network
 Ecoreach software
 FDM128 display

Two passwords are defined:

 the level 3 password
 the level 4 password

The level 4 password is required to write the settings to the Micrologic control unit using the Ecoreach software.

Each intrusive command via the command interface is protected by a password. The password level for each intrusive command is indicated in the description of the command.

No password is required for non-intrusive commands through the command interface.
 
Was this helpful?
What can we do to improve the information ?