Technical FAQs

Ask a Question

How do you install the 8501NH7 strap?

Issue:
Adding the retaining strap onto the 9050JCK timer on the base.

Product line:
9050 JCK timer

Environment:
all

Cause:
Installation

Resolution:
The spring clip secures onto the side of the timer base.  See attached.
Was this helpful?
What can we do to improve the information ?