Technical FAQs

Ask a Question

How to enable and disable the IEC 61850 Server in BMENOP0300 module?

Use the controls in the Server Function section to enable and disable the IEC 61850 server.
The Server Function section presents the following settings:

Was this helpful?
What can we do to improve the information ?