Technical FAQs

Ask a Question

How to enable and disable the IEC 61850 Client in BMENOP0300 module?

Use the controls in the Server Function section to enable and disable the IEC 61850 client.
The client function section presents the following settings:

Was this helpful?
What can we do to improve the information ?