Technical FAQs

Ask a Question

What schema versions are supported by the IEC 61850 configurator tool used for BME NOP 0300 Module configuration in Unity Pro

The IEC 61850 configurator editions support the following schema versions:
 Edition1: supports schema V1.6
 Edition2: supports schema V3.1
Was this helpful?
What can we do to improve the information ?