Technical FAQs

Ask a Question

Creating a New Server from an External Schneider Electric ICD / CID File in the 'IEC 61850 configurator' used for BME NOP 0300 module configuration in Unity Pro

You can create a new server instance from an ICD or CID file that was previously created and saved using the Modicon IEC 61850 Configuration Tool. To create a new server from an external ICD or CID file, follow these steps:
Was this helpful?
What can we do to improve the information ?