Technical FAQs

Ask a Question

Creating a New Server from an SCD File in the 'IEC 61850 configurator' used for BME NOP 0300 module configuration in Unity Pro

The Modicon IEC 61850 Configuration Tool can create a new server from an IED file contained in an external SCD file. To create a new server from an external SCD file, follow these steps:
Was this helpful?
What can we do to improve the information ?