Technical FAQs

Ask a Question

Deleting an existing server in the 'IEC 61850 configurator' used for BME NOP 0300 module configuration in Unity Pro

You can delete the IEC 61850 server instance that is currently displayed in IEC 61850 Server window. To delete the server, follow these steps:
Was this helpful?
What can we do to improve the information ?