Technical FAQs

Ask a Question

Exporting the server to a CID or ICD file in the 'IEC 61850 configurator' used for BME NOP 0300 module configuration in Unity Pro

You can export the IEC 61850 server instance that is currently displayed in IEC 61850 Server window, as a CID or ICD file. To export a server, follow these steps:

Was this helpful?
What can we do to improve the information ?