Technical FAQs

Ask a Question

Exporting the Server to an Excel Spreadsheet file from the 'IEC 61850 configurator' used for BME NOP 0300 module configuration in Unity Pro

You can export the configured IEC 61850 server that is currently displayed in IEC 61850 Server window, as an Excel 97-2003 spreadsheet file. To export a server, follow these steps:
  1. Click the Export to Excel button. Result: The Save As dialog opens.
  2. In the Save As dialog:
     Navigate to the location where you want to save the exported file.
     Click Save.
The exported Excel spreadsheet file populates the following fields with configured server data:
 Reference: the path and name of the data item
 BasicType: the data type of the item
 FC: the functional constraint value of the data item
 DO/DA: the type of item: data object (DO) or data attribute (DA)
 Initial Value: The initialized value assigned to the data item
All other fields in the spreadsheet are not populated.
 
Was this helpful?
What can we do to improve the information ?