Technical FAQs

Ask a Question

How many report control block instances are supported by BMENOP0300 module

The IEC 61850 server in the BMENOP0300 module supports:
 up to 64 buffered or unbuffered report control block instances within a single IED
 up to 8 instances of a single buffered control block, which can be transmitted to 8 clients, upon the occurrence of possibly different triggering conditions
Was this helpful?
What can we do to improve the information ?