Technical FAQs

Ask a Question

What is the part number of CANopen card for ATV320 drives.

ATV320 comes as standard with both Modbus and CANopen communication port protocol.
CANopen protocol is integrated on ATV320 as a standard;So,there is no optional card for CANopen.


 
Was this helpful?
What can we do to improve the information ?