Technical FAQs

Ask a Question

What is the accuracy of Analog Input and Analog output on ATV630 drives.

+/- 0.6 % AI1, AI2, AI3 for a temperature variation 60 °C analog input
+/- 1 % AO1, AO2 for a temperature variation 60 °C analog output

Where  AI = Analog Input
             AO = Analog Output



 
Was this helpful?
What can we do to improve the information ?