Technical FAQs

Ask a Question

Do the Everlink reversing contactors come with electrical interlocking?

Issue:
Looking for electrical interlock kit for the LC1D65A Everlnk contactors

Product line:
Tesys D LC1D40A, LC1D50A, LC1D65A

Environment:
Everlink, all voltage codes

Cause:
Old D2 version offered an electrical interlock kit

Resolution:
The current Everlink version does not offer an electrical interlock kit.  The customer can wire electrical interlocking using the normally closed contacts provided on the contactor.
Was this helpful?
What can we do to improve the information ?