Technical FAQs

Ask a Question

How do I use/wire the TeSys Island Digital IO module?

Issue:  
How is the TeSys Island IO wired? 

Product Line: 
Tesys Island

Environment:
Digital multifunctional load management solution 
 
Resolution:
  • The digital inputs require an externally supplied 24V signal to drive them high. Simply shorting I0 to IC will not drive the input high.
  • The digital outputs will connect and disconnect an externally supplied 24V source. The 24V is not derived from the island itself, it must be supplied by the user
Was this helpful?
What can we do to improve the information ?