Technical FAQs

Ask a Question

Can I use single phase and three phase in my system with TeSys Island?

Issue:  
Utilizing single and 3 phase motors in the same Island. 

Product Line: 
Tesys Island

Environment:
Digital multifunctional load management solution 
 
Resolution:
Yes, you can use a mixture of single phase and three phase Avatars in your system. If doing this, you must configure the "island" (VIM) as three-phase, and wire it A-B-C. Then for any single-phase avatars, they must be wired with phase A in the line 1 connection and phase C in the line 3 connection. The single-phase voltage must be Line-Line. At the moment TeSys island does not support energy monitoring for single-phase voltages L-N if the entire system is three-phase.
Was this helpful?
What can we do to improve the information ?