Technical FAQs

Ask a Question

Are the Altivar 320 drives Plenum rated?

Issue:
Wants to mount the drive in the Plenum

Product line:
ATV320, Altivar 320 Machine drives

Environment:
all

Cause:
Mounting and installation

Resolution:
The ATV320 drives are not plenum rated.
 
Was this helpful?
What can we do to improve the information ?