Technical FAQs

Ask a Question

Can I hot-swap the bus devices in TeSys Island?

Issue:  
Does TeSys Island support hot-swap

Product Line: 
Tesys Island

Environment:
Digital multifunctional load management solution 
 
Resolution:
No, the island must be powered off to add or remove devices to the internal bus. However, thanks to fast device replacement if you are replacing only bus devices and keeping the bus coupler, the bus coupler will synchronize the new device to the appropriate firmware version and start working with it immediately upon power-up.
Was this helpful?
What can we do to improve the information ?