Technical FAQs

Ask a Question

Can I use TeSys island in a Ring Topology?

Issue:  
Does TeSys Island support ring topology

Product Line: 
Tesys Island

Environment:
Digital multifunctional load management solution 
 
Resolution:
Yes, RSTP is enabled by default when storing a configuration from the DTM. Make sure to use the 2 fieldbus ports, as it is not enabled for the top Service port.
Was this helpful?
What can we do to improve the information ?